ESP32-C5 for Home Assistant: Why Choose It Over ESP32-C6 for Smart Home Projects?
By Josie 5 months agoESP32-C6 has become the default choice for many ESPHome and Home Assistant projects—but where does ESP32-C5 fit? This guide compares ESP32-C5 vs ESP32-C6, explores ESPHome compatibility, and shows how XIAO ESP32-C5 can be used to build modern smart home devices.
ESP32-C6 Has Become the Default Choice for Smart Home Projects
ESP32-C5 vs ESP32-C6: What's Actually Different?
| Feature | ESP32-C5 | ESP32-C6 |
|---|---|---|
| CPU | Single-core RISC-V, up to 240 MHz | Single-core RISC-V, up to 160 MHz |
| Wi-Fi 6 | ✅ | ✅ |
| 2.4 GHz Wi-Fi | ✅ | ✅ |
| 5 GHz Wi-Fi | ✅ | ❌ |
| Bluetooth LE 5.x | ✅ | ✅ |
| IEEE 802.15.4 | ✅ | ✅ |
| Matter Support | ✅ | ✅ |
| Thread Support | ✅ | ✅ |
| Zigbee Support | ✅ | ✅ |
| Smart Home Ecosystem Maturity | Growing | Mature |
| Typical Smart Home Usage Today | Emerging | Widely adopted |
Which One Should Smart Home Builders Choose?
- Choose ESP32-C6 for proven smart home deployments and maximum community support.
- Choose ESP32-C5 when your project can take advantage of 5 GHz connectivity and enhanced networking flexibility.
Why 5 GHz Wi-Fi Matters More Than You Might Think?
Escaping Crowded 2.4 GHz Networks
More Reliable Connectivity for Smart Home Dashboards
Better Fit for Data-Intensive Devices
Bringing ESP32-C5 into the Smart Home Ecosystem
Connecting ESP32-C5 with Home Assistant
Native ESPHome Integration
Zigbee and Thread Devices
Matter Devices
Why ESPHome Is the Most Popular Option
What Can You Build with ESP32-C5 Today?
Sensor nodes
Bluetooth Proxy
Why Many Developers Choose XIAO ESP32-C5
From ESPHome to Home Assistant: Getting Started with XIAO ESP32-C5
Build Faster with the Pre-Soldered Version
If you want to prototype quickly, the Pre-Soldered version of XIAO ESP32-C5 lets you skip header soldering and start building immediately. It plugs directly into XIAO expansion boards and breadboards, making it especially suitable for beginners, rapid prototyping, and iterative smart home development.
Expand with Grove Sensors
XIAO ESP32-C5 is also part of the broader Grove ecosystem. By pairing it with Grove sensor modules—such as temperature & humidity sensors, air quality sensors, mmWave radar, displays, buttons, and relay modules—you can assemble smart home prototypes with minimal wiring and quickly integrate them into ESPHome and Home Assistant.
Looking Ahead: The Untapped Potential of ESP32-C5 in Smart Homes
Beyond Sensors and Switches
Opportunities for Camera-Based Devices
Conclusion
Notes at the end.
Hey community, we’re curating a monthly newsletter centering around the beloved Seeed Studio XIAO. If you want to stay up-to-date with:
🤖️ Cool Projects from the Community to get inspiration and tutorials
📰 Product Updates: firmware update, new product spoiler
📖 Wiki Updates: new wikis + wiki contribution
📣 News: events, contests, and other community stuff
Please click the image below👇 to subscribe now!