Meet XIAO nRF54LM20A (Sense): Motion Wake-Up. Always Connected. Built for Ultra-Low Power

Introducing Seeed Studio XIAO nRF54LM20A (Sense): Nordic nRF54LM20A Board for Matter, Thread & Ultra-Low-Power IoT. It features Bluetooth LE 6.0, Matter, Thread, Zigbee, 28 GPIOs, 2 MB Flash, 512 KB RAM, and optional IMU and microphone for battery-powered IoT, wearables, and edge sensing applications.

Seeed Studio XIAO family has always been shaped by how the community actually uses it. Following the debut of XIAO nRF54L15 and XIAO nRF54L15 Sense, developers are now looking for lower power consumption that holds up in real deployments, more GPIOs for system-level integration, and more seamless wireless design, including antenna switching and NFC in compact layouts. At the same time, applications are becoming more sophisticated, requiring greater memory capacity and processing headroom.

Today, we’re excited to introduce Seeed Studio XIAO nRF54LM20A and XIAO nRF54LM20A Sense. Built around Nordic Semiconductor’s new nRF54LM20A platform and paired with the nPM1300 PMIC, this new XIAO series delivers ultra-low power, high performance, expanded IO, and richer integration — all within the signature XIAO footprint. 

Both boards are now available for pre-order via our official Bazaar Webstore and AliExpress Store, with early bird pricing starting from USD $8.90 and USD $14.90 respectively.

Key Features at a Glance

  • Power-Optimized Architecture: Nordic’s nRF54LM20A SoC with nPM1300 PMIC, aligned with Nordic’s reference EVB design in XIAO Form Factor
  • Large Memory Capacity: 2036 KB NVM + 512 KB RAM, with an additional 8 MB external memory
  • Multiple Connectivity: BLE 6.0, Matter, Thread, Zigbee, and proprietary 2.4 GHz (up to 4 Mbps) with efficient multi-protocol operation
  • Thumb Size with Rich Peripherals: 28 GPIOs, USB Type-C, onboard battery charging, and SMD-friendly design for production integration
  • Extra Sensors on the Sense version: Built-in digital microphone and 6-axis IMU with motion-triggered wake-up for ultra-low power applications
  • Low-Power RGB LED Design: Diode RGB LEDs directly controlled by GPIOs for zero standby power consumption
  • Optimized Antenna & NFC System: Improved RF routing and practical onboard NFC integration

Bringing EVB-Level Performance into the XIAO Form Factor

Low power in real applications is not defined by the MCU alone. With XIAO nRF54LM20A (Sense), we‘ve worked closely with Nordic Semiconductor and aligned with their official EVB reference design, integrating the npm1300 PMIC with its recommended configuration. This is important because the official EVB design represents a validated, optimized baseline for how the nRF54LM20A should perform, and now you can have performance and power behavior that are much closer to Nordic’s EVB in a thumb-sized XIAO.

The integration of npm1300 also enables features such as shiphold mode, allowing the system to enter a true near-zero power state during storage or transport, preventing unintended battery drain before deployment.

Image Source: Nordic

Eliminating Hidden Power Costs

Even small hardware decisions can have a measurable impact. With XIAO nRF54LM20A (Sense), we use R/G/B LEDs instead of addressable LEDs, eliminating standby current from LED drivers entirely. Unlike typical addressable LEDs that require continuous power to maintain state, this design ensures zero power draw when LEDs are off, while still providing full control through GPIOs.

In our internal testing using Nordic’s Power Profiler Kit II (PPK2), the board achieved a System OFF current as low as 4.93 μA when powered by a 3.7 V Li-ion battery. (We’ll be sharing more behind-the-scenes stories and low-power design details of the XIAO nRF54LM20A in a future technical blog—stay tuned!)

On the Sense version, the onboard 6-axis IMU is connected to a wake-up capable pin, allowing the device to remain in deep sleep and wake instantly on motion. This has a direct impact especially on wearables, motion-triggered edge devices, and always-on sensing scenarios.

More IO, More Integration

The XIAO nRF54LM20A (Sense) adopts the Plus form factor, expanding to 28 GPIOs while remaining compact, giving developers more flexibility when building complete systems. It is also designed with SMD integration in mind, making it easier to move from development to production.

Beyond IO, the board integrates essential system components directly onboard, including USB Type-C, battery charging circuitry, Reset and User buttons, and an IPEX antenna connector for flexible RF deployment. NFC has also been further optimized for onboard use, making features like tap-to-connect and device provisioning more practical in compact designs. Together, these improvements reduce the need for external components and simplify hardware design.

(Hardware Overview of XIAO nRF54LM20A Senes)

XIAO nRF54LM20A (Sense) VS XIAO nRF54L15 (Sense) VS XIAO nRF52840 (Sense)

Product NameXIAO nRF54LM20AXIAO nRF54LM20A SenseXIAO nRF54L15XIAO nRF52840
ProcessorArm® Cortex®-M33, 128 MHz
RISC-V,128 MHz (Coprocessor)
Arm® Cortex®-M33, 128 MHz
RISC-V,128 MHz (Coprocessor)
Arm® Cortex®-M33, 128 MHz
RISC-V,128 MHz (Coprocessor)
ARM®Cortex®-M4 32-bit processor with FPU, 64 MHz
Software CompatibilityNordic nRF Connect SDK,PlatformIO, ZephyrNordic nRF Connect SDK,PlatformIO, ZephyrNordic nRF Connect SDK,PlatformIO (Zephyr)Arduino IDE, PlatformIO, MicroPython, CircuitPython, Zephyr
Wireless ConnecticityBluetooth LE 6.0 (include Channel Sounding), Bluetooth Mesh, NFC, Thread, Zigbee, Matter, Amazon Sidewalk, Proprietary 2.4 GHz protocolsBluetooth LE 6.0 (include Channel Sounding), Bluetooth Mesh, NFC, Thread, Zigbee, Matter, Amazon Sidewalk, Proprietary 2.4 GHz protocolsBluetooth LE 6.0, Bluetooth Mesh, Zigbee, Thread, Matter, Amazon Sidewalk, and proprietary 2.4 GHz protocols.Bluetooth LE 5.4, NFC, Zigbee, proprietary 2.4 GHz protocols
InterfaceGPIO(PWM)Pin x28
Digital Pin x28
Analog Pin x8
I2C x2
UART x1
SPI x2
GPIO (PWM) Pin x26
Digital Pin x26
Analog Pin x8
I2C x1
UART x1
SPI x2
GPIO(PWM)Pin x16(Sense version is14)
Digital Pin x16
Analog Pin x6
I2C x2
UART x1
SPI x2
GPIO(PWM)Pin x11
Digital Pin x11
Analog Pin x6
I2C x1
UART x1
SPI x1
OnboardUser R/G/B LED x1
Charge LED (Red) x1
Reset Button x1
User Button x1
1x IPEX Connector (for external antenna)
User R/G/B LED x1
Charge LED x1
Reset Button x1
User Button x1
1x IPEX Connector (for external antenna)
6-Axis IMU x1
Mic x1
User LED x1
Charge LED x1
Reset Button x1
User Button x1
Onboard Ceramic Antenna x1
U.FL Connector (for external antenna) x1
User LED x1
Charge LED x1
Reset Button x1
BlueTooth Antenna x1
Price$9.90 (early bird $8.90)$15.90 (early bird $14.90)$9.9$9.9

Where to Get Started

The XIAO nRF54LM20A and XIAO nRF54LM20A Sense (with both the standard variants and pre-soldered variants) are now live for pre-order at USD $8.90 and USD $14.90 respectively via our official Webstore Bazaar and AliExpress Store, with shipping starting from 15, July, 2026. 

To help you get started quickly, we’ve prepared a comprehensive set of technical resources, including hardware documentation, getting-started guides and development tutorials. Explore the wiki to begin building with XIAO nRF54LM20A (Sense) today.

End Note

We’re curating a bi-weekly newsletter centering around the beloved Seeed Studio XIAO. If you want to stay up-to-date with cool projects from the community, product and Wiki updates, news, etc., please click here to subscribe now!

About Author

Calendar

June 2026
M T W T F S S
1234567
891011121314
15161718192021
22232425262728
2930