Which Robotic Arms are Compatible with Pi0.5?

Any robotic arm with a LeRobot robot class can run a fine-tuned Pi0.5 (π0.5) policy, because π0.5 is implemented in LeRobot as the policy type pi05 and adapts automatically to your robot’s motor states, motor actions, and number of cameras — this information is stored in the LeRobot dataset you record.

Robotic Arms Recommendation to Train and Run Pi0.5

Seeed Studio reBot Arm B601-DM, reBot Arm B601-RS, and SO-ARM101 are verified to run π0.5 fine-tuning end-to-end.
 
Check out this GitHub tutorial to see how Pi0.5 (π0.5) is deployed across these three robotic arms, complete with a full step-by-step guide.
Robotics arm support pi0.5

Why are the reBot Arm Series and SO-ARM101 recommended for running Pi0.5?

  1. Verified End-to-End Pi0.5 Workflow: All three models are fully verified in LeRobot (pi05 policy) with dedicated robot classes, ready-to-use CLI commands, and compatible camera mounts—taking you smoothly from calibration and teleoperation to dataset recording, fine-tuning, and real-arm deployment.
 
  1. Hardware Tiers for Every Budget & Need:
  • SO-ARM101: Ultra-low-cost entry point powered by Feetech serial servos (so101_follower). Payload < 200 g, ideal for budget-conscious beginners.
  • reBot Arm B601-DM: Low-cost, high-value robotic arm, plug-and-play, a drop-in replacement for YAM and Openarm with identical joint actuators. Payload: 1.5 kg (without gripper). Matches with the reBot Arm 102 leader.
  • reBot Arm B601-RS: High-rigidity structure equipped with RobStride RS QDD actuators — high burst torque, high responsiveness, higher payload. Payload: 2.5 kg continuous / 5 kg peak (without gripper), with native SocketCAN (can0) / PCAN support for demanding control tasks.
 
  1. 100% Open-Source & Commercially Friendly: Unlike costly proprietary bimanual platforms, the reBot Arm series is 100% open-source robotic arm (commercial use and reproduction allowed), drastically lowering the barrier to deploying VLA models.
 
  1. No-Code & Free Training Ecosystem: Both series work out of the box with free Seeed AI Robotics Academy tutorials and the SenseCraft Robotics desktop client, enabling no-code data collection and cloud training without needing a local GPU.

How to choose?

In short, choose SO-ARM101 for the easiest, lowest-cost Pi0.5 entry. reBot Arm B601-DM for plug-and-play USB-CAN robotic development. And reBot Arm B601-RS for high-rigidity, SocketCAN-based deployment.

See it run

Learn how to use SenseCraft Robotics with SO-ARM and π0.5 through a desktop tidying example. This tutorial walks through arm and camera setup, teleoperation data collection, dataset review and merging, cloud training, and running the trained model.

References

FAQ

Could not connect on port /dev/ttyUSB0 or /dev/ttyACM0

you forgot serial permissions: sudo chmod 666 /dev/ttyUSB* /dev/ttyACM*.

No valid stream found in input file

install ffmpeg 7.1.1: conda install ffmpeg=7.1.1 -c conda-forge.

How long does training take?

Fine-tuning π0.5 for 3000 steps takes a few hours on an RTX 4090 / A100; smaller GPUs work with train_expert_only=true + reduced batch_size, or use cloud training / SenseCraft Robotics.

The arm fails to grasp after training

check data quality first: camera positions, angles and lighting must stay stable during collection; reduce background changes and pedestrians in frame; verify the object was visible in both cameras; and record enough episodes (50+).

Keyboard shortcuts don't respond during recording

downgrade pynput: pip install pynput==1.6.8 (and verify $DISPLAY is set).

Camera image errors

do not connect USB cameras through a hub; plug them directly into the machine.

Which repository should I clone?

Use https://github.com/Seeed-Projects/lerobot.git (the verified fork this tutorial targets). The upstream huggingface/lerobot moves fast and may differ in dataset versions and commands.

Software or environment issues you can't resolve?

Check the LeRobot GitHub issues( https://github.com/huggingface/lerobot ), join the LeRobot Discord ( https://discord.gg/8TnwDdjFGU ), or the Seeed discussion ( https://github.com/Seeed-Studio/wiki-documents/discussions/69 ).

About Author

Leave a Reply

Your email address will not be published. Required fields are marked *

Calendar

November 2026
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
30