News

news – product updates
news – events
news – news letter

Meet the First Batch of 27 Winners to Get a Free Seeed Studio LoRaWAN Dev Kit: Time to Submit Your Ideas to Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022”

Currently, Seeed Studio is running “IoT Into the Wild Contest for Sustainable Plant 2022” on Hackster.io. So far, we’ve received 45 free hardware applications, along with 200+ people registered as the Contest participants. In an effort to inspire a broader number of potential participants, as well as to facilitate the makers and innovators to start their projects early-on, we’ve selected 27 free hardware applicants to send out Seeed Studio LoRaWAN Dev Kit next week.

July 2022: Seeed’s Field Application Engineer Will Be at Dinacon 3 in Sri Lanka for Wild Hacking for a Holistic #IoTIntoTheWild Project Implementation!

To continue the discourse and our efforts on wildlife, biodiversity, and environmental conservation, we’d like to share a good news that Seeed’s Field Application Engineer, Lakshantha Dissanayake, will be joining the 3rd edition of The Digital Naturalism Conference in Batticaloa, Sri Lanka from July 1st to 10th, 2022.

Join Seeed’s “IoT Into the Wild Contest for Sustainable Planet 2022” on Hackster to Get 100 Free Hardware and to Win $14,000+ in Prizes!!

Together with Hackster.io, we are very happy to jointly organize “IoT Into the Wild Contest for Sustainable Plant 2022”, which is supported by Project 15 from Microsoft, Zambezi Partners, Edge Impulse, Fab City Foundation, Institute for Advanced Architecture of Catalonia (IAAC), the Paradise International Foundation, Nova Labs, and Helium. We hope that open tech can lay an important foundation for achieving the UN’s Sustainable Development Goals. Through the contest, we hope to encourage more applicable, scalable, plug-and-play, and easy-to-deploy AIoT solutions to solve real-life challenges in the wild.

Calendar

December 2025
M T W T F S S
1234567
891011121314
15161718192021
22232425262728
293031