Forum

Seeed Participates in Tsinghua University-Led “SDG Open Hack” as a Mentor and Sponsor for Students’ Smart and Sustainable Community Projects

To encourage and foster an environment where university students’ creativity, enthusiastic hearts, and innovative solution ideas on sustainable development challenges can be nurtured, “SDG Open Hack” has been organized annually since 2019. Ever since the Hack was held, Seeed Studio has been an engaged partner to contribute to the advancement of SDGs in the academic realm through mentoring and sponsoring open source hardware products. In this two-day event, students came up with innovative solutions on elderly care, waste management, digital recycling, cultural heritage protection, and shared economy, by incorporating the application of science and technology. Thereby, SDG Open Hack sought to achieve the UN’s SDGs 4, 12, 11, 17, 5, 9, 13 and 16.

Janwaar Maker Space in the Making: Seeed’s Open Source Hardware for Rural Changemakers’ Self-Empowerment and Social Inclusion in India

In an effort to assist decentralization of digital education for rural children in India, Seeed donated open hardware products to Janwaar village, where the children and youth were inspired to learn coding and programming for the first time in their lives. Through embracing the learning principle of hands-on, DIY, and collaborative learning, they were self-empowered to have the ownership of technological tools, and to tackle gender inequality and casteism at village level. On this backdrop, this “Janwaar Maker Space in the Making” Project directly or indirectly accelerates the UN’s SDGs 4, 5, 10, 11, 9, 1, 17, 8 and 16.

Open Innovation for Marine Pollution: Wind-Powered Sailing Robot “Protei” Is Cleaning Oil Spills, Material Wastes, and Chemical Pollutants in the Ocean

In order to resolve the world’s oil spill issues caused by the Deepwater Horizon Disaster in the Gulf of Mexico, Protei (a wind-powered and automated sailing fleet robot) was developed by MakerBay and Seeed. By shifting its shapes according to water waves and wind directions, the robot has been useful in collecting and cleaning thin sheens of light oil on water surfaces. Thanks to the fact that it is robustly built to survive in harsh weather conditions and hazardous chemical zones, it is now also used to clean material wastes and other chemical pollutants in the ocean. Now, Protei is the ongoing result of glocal open innovation communities. Accordingly, this Project seeks to achieve the UN’s SDGs 6, 14, 11, 15, 3, 1, 7, 9, 8, 12, 13 and 17.

Calendar

January 2026
M T W T F S S
 1234
567891011
12131415161718
19202122232425
262728293031