PCBA Firmware Programming Guide: Methods, Workflow, and Verification
A programming tool can report a successful write even when the application does not start. To check the result, look at three stages separately: connecting to the chip, verifying the programmed data, and checking that the application runs as expected.
Firmware programming writes a compiled program into a chip’s memory. Using microcontroller-based boards as examples, this guide explains how to choose an interface and tools, interpret verification and startup results, and troubleshoot problems at each stage. It also covers connections, firmware versions, and verification requirements when moving from prototypes to production.
Jump to the section you need:
- Where Firmware Is Stored
- Choosing a Programming Method
- The Firmware Programming Workflow
- Common Problems and Troubleshooting
- Moving from Prototypes to Production
- Adding Firmware Programming to a PCBA Order
💾Where Firmware Is Stored
Firmware is usually stored in nonvolatile memory, which retains its contents when power is removed. Some MCUs contain internal Flash memory, while other designs use a separate Flash chip. The chip model and board design determine where the firmware is stored and how it can be programmed. STM32F401 devices and the Raspberry Pi RP2040 illustrate these two approaches: internal Flash and external Flash.
Source code is typically compiled into files that a programming tool can load. Common formats include BIN and HEX. A BIN file contains binary data, with the destination address usually specified separately in the programming settings. An Intel HEX file can include address information. Supported formats and address handling depend on the tool.
A project may also require several files. An ESP-IDF project, for example, can generate separate binaries for the bootloader, partition table, and application. Each must be written to the correct location. Having the complete set of files and the correct addresses is essential.
IC programming also covers other devices. EEPROM may hold settings or calibration data, while FPGA and CPLD programming involves configuration data that defines logic functions. Files and programming methods vary by device. The workflow below focuses on MCU firmware.
Whether programming is needed depends on the product’s functions and the components used. For a programmable controller, check whether it already contains suitable firmware or needs to be programmed or updated during production.
🔌 Choosing a Programming Method
This section focuses on programming devices after they have been assembled onto a PCB. Firmware reaches the target device through a connector or contact points on the board. Choosing a method starts with checking which programming interfaces the chip supports and how those interfaces are connected.
| Interface or method | How it works | What to check |
| SWD | A compatible debug probe or programmer accesses the target device through its SWD interface. This is an option for some STM32 and other MCUs. | Support for the exact chip model, tool compatibility, pin connections, and target voltage. |
| JTAG | A compatible tool connects to the device’s JTAG interface for supported programming and debugging operations. | Device programming support, signal connections, and tool settings. |
| Firmware download over UART, USB, or another supported interface | A built-in download program or previously installed bootloader receives the firmware and writes it to memory. | Available download interfaces, bootloader support, and how to enter download mode. |
Support varies by device. STM32CubeProgrammer, for example, can access compatible devices through SWD and JTAG, or through bootloader interfaces such as UART and USB DFU. An individual STM32 model may support only some of these options.
A USB connector alone does not establish that a board supports firmware programming over USB. Its data lines must connect to a supported download interface, either directly or through suitable conversion circuitry. The chip also needs a working download mechanism. Some chips include a download program from the factory; other designs require a bootloader to be installed first.
Use the exact chip model and board schematic to identify the available interface, required connections, and conditions for entering programming mode. Then choose compatible software and hardware. The chip datasheet and manufacturer’s programming documentation provide the relevant requirements.
🛠️ The Firmware Programming Workflow
Before starting, it helps to understand what each part of the setup does. Some functions require separate equipment; others may already be built into the board.
| Tool category | Main purpose | Common examples |
| Programming software | Loads files, selects the target, sets parameters, and runs programming and verification. | STM32CubeProgrammer, esptool. |
| Programming or communication hardware | Connects the computer to an interface supported by the target device. | An ST-LINK debug probe, or USB-to-UART circuitry for serial downloading. |
| Cables, adapters, and fixtures | Connect signals to the required pins or contact points. A fixture can also hold the board in position. | Ribbon cables, adapter boards, probe fixtures. |
These parts must work together with the selected programming method. Some ESP32 development boards include a USB-to-UART bridge, allowing the computer to communicate with the chip through a USB connection. An SWD setup can instead use an external debug probe connected to the target MCU.
Figure caption: SWD programming example: a computer connects to a debug probe over USB, and the probe accesses the MCU’s internal Flash through SWD. This is a functional overview; refer to the hardware documentation for wiring.
A typical programming operation includes the following steps. Commands and their exact order depend on the platform.
- Identify the target and firmware. Check the chip model, board revision, firmware version, required files, and destination addresses.
- Connect the board. Check power, ground, and signal connections against the requirements for the selected interface.
- Configure the tool and connect to the target. Select the device, port, or debug interface, set the required parameters, and enter download mode or reset the device as instructed.
- Program the device. Perform the required erase, configuration, and write operations. Keep the complete tool output.
- Check verification. Use the tool’s supported verification function to check the programmed data against the expected contents.
- Restart and check operation. Reset or power-cycle the board as required, then check serial output, version information, or the agreed functional response.
Espressif’s ESP-IDF hello_world example for ESP32 shows why these stages matter. The build produces several binaries, which the tool writes to their assigned addresses. The example output provides three distinct checks:
| Output excerpt | What it shows |
| Connected to ESP32 | The tool has connected to the target. |
| Hash of data verified. | Verification passed for the corresponding programmed data. |
| Hello world! | The example application has started and printed a message. |
The official guide shows the programming log separately from the application’s serial output, illustrating the difference between writing firmware and running it.
These messages belong to a specific example, tool version, and hardware setup. Other platforms may report results differently. Check connection, data verification, and application startup separately. Sensors, communication, and other required functions need their own tests.
🔎 Common Problems and Troubleshooting
Programming problems can usually be grouped by when they occur: connection, writing, verification, or application startup. Each stage has different checks. The table below gives general troubleshooting directions; use the device and tool documentation for specific settings.
| Symptom | What to check first |
| Target cannot be detected or connected | Device and port selection, whether another application is using the port, power, ground, signal connections, and boot or reset conditions. |
| Programming stops partway through | Contact quality, cables, power stability, and communication settings. Try a lower communication speed if recommended by the manufacturer. |
| Verification fails | The exact error message, write and verification settings, and the reliability of power and connections. |
| Programming completes, but the application does not run | Firmware and hardware compatibility, missing files, destination addresses, boot settings, and power during normal operation. |
Espressif’s ESP32 troubleshooting documentation gives two useful examples. An unsuitable Flash mode can allow programming to finish while preventing the application from booting. A power supply may also support downloading but fail to meet the application’s operating requirements. Startup logs and hardware checks help investigate these cases.
Complete error messages, tool versions, firmware versions, and board revisions make problems easier to reproduce. If only some boards in a batch fail with the same firmware and tool settings, comparing passing and failing boards can help identify differences in contact quality, power, or assembly.
🏭 Moving from Prototypes to Production
As quantities increase, every board needs to be connected, programmed, and checked. Production preparation needs to establish which firmware version belongs to each board revision and make the procedure and acceptance criteria repeatable.
Successful programming on one board is only part of the task. Repeated connections also need to be practical and reliable. Programming connectors or contact points must remain accessible after assembly, with enough clearance from tall components, heatsinks, and enclosures.
Whether a fixture is useful depends on production quantity, connection type, and how often the operation is repeated. A fixture can hold the board and position probes against the same contact points. Programming several boards simultaneously also requires suitable programming channels and a setup that supports parallel operation.
For more on fixtures and test systems, see the Seeed Fusion Modular PCBA Testing Guide.
📩 Adding Firmware Programming to a PCBA Order
If you want your boards delivered with specific firmware already installed, request programming when arranging PCBA production with Seeed Fusion. Fusion can program the supplied firmware before shipment according to the agreed requirements. Common requests include programming XIAO or other development boards used on a customer’s PCBA.
Provide the firmware files and describe the expected result after programming. For example, a single buzzer beep at power-up could serve as an agreed startup check. If sensor readings or communication functions also need to be checked, specify the test method and expected results. Programming and verification requirements should be agreed before production.
Simple programming with few special requirements is generally available at no extra charge as part of a PCBA order. More complex requests that require additional time or resources need a separate cost assessment. For other production changes based on XIAO, explore the XIAO customization service.
Email [email protected] with the board details, quantity, firmware files, and verification requirements. Include your order number if you have already placed an order. If you have a working programming procedure, share it to help confirm the arrangements.