Tire Care device with machine learning based on Seeed Studio XIAO nRF52840 Sense
With Machine Learning it is possible to teach the device what is a “regular” break
With Machine Learning it is possible to teach the device what is a “regular” break
SAJAC is an innovative smart jacket designed specifically for caving expeditions. This jacket incorporates advanced
A coffee grinder is great for grinding coffee, but what if you wanted to produce
Saltwater intrusion is a significant problem for rice paddies in Vietnam, as seawater is increasingly
The device is HID mouse controller with 4 buttons. There are: left mouse click, right
Hey community, I’m excited to share that Seeed Monthly is back with a new
On March 15th, Seeed Studio was awarded “WSIS Prize 2023 Champion” prize certificate at the UN ITU, in Geneva, Switzerland. It’s a UN-level of recognition for the success of IoT2Wild Contest 2022 and the usage of ICTs for environment, which was awarded at ITU’s 14th World Summit on the Information Society (WSIS) Forum 2023.
Need to add WiFi to your project? Consider the WizFi360 WiFi module now in a
The Grove system consists of open-source, plug-and-play hardware for modular electronics project building. By providing
17 Goals to Change the World. The 17 Sustainable Development Goals (SDGs) are an important part
The greenhouse and poultry farming can use sensors to monitor and control environmental parameters for
Bauta delivered powerful edge video analysis solutions to provide business organizations and local departments an