reBot Arm B601-RS Performance & Durability Tests: Payload, Repeatability, Teleoperation and Gravity Compensation
Open-source robot arms are increasingly becoming an important platform for Physical AI, imitation learning, robotics research, and lightweight automation.
But specifications alone do not determine whether a robot arm is ready for real-world development.
For developers collecting hundreds or thousands of demonstrations, running repeated manipulation tasks, or building autonomous robotic systems, several questions matter just as much:
- Can the arm follow high-speed teleoperation commands smoothly?
- Can it maintain stable motion under realistic payloads?
- Does positioning remain consistent after repeated operation?
- Can the mechanical structure withstand frequent interaction and handling?
- Does the control system provide the compliance required for physical AI applications?
To evaluate these questions, Seeed Studio put the reBot Arm B601-RS through a series of performance and durability-oriented tests covering teleoperation, payload capability, repeatability, gravity compensation, and mechanical construction.
The goal is straightforward: evaluate how the B601-RS performs beyond the specification sheet and under conditions closer to real robotics development.
High-Speed Teleoperation for Physical AI Data Collection
Teleoperation is becoming one of the most important workflows in Physical AI.
Frameworks such as LeRobot use human demonstrations to collect manipulation trajectories that can later be used to train imitation-learning and robot-learning policies. In these workflows, teleoperation latency and motion quality directly affect the quality of the collected dataset.
The reBot Arm B601-RS supports leader-follower teleoperation through CAN communication.
For the test setup, the B601-RS follower arm was paired with a StarArm 102-L leader arm, using:
- CAN bus communication at 1 Mbps
- MIT motor control mode
- 125 Hz control update rate
- Position, velocity, acceleration, and jerk constraints

Test Result
During fast sweeps, slow positioning movements, and rapid direction changes, the follower arm maintained responsive tracking of the leader arm without obvious oscillation or overshoot.
The control performance is supported by the B601-RS actuator architecture, which combines:
- 4 × RobStride RS-00 motors
- 3 × RobStride RS-06 motors
- Quasi-direct-drive actuator design
- High-torque output with low mechanical resistance
This configuration helps provide smoother motion than conventional high-ratio geared architectures while maintaining the torque required for manipulation tasks.
The gripper additionally supports impedance-based control, allowing grasping force to be constrained during interaction with objects.
Why It Matters
Responsive teleoperation is not only about making the robot easier to control.
For Physical AI developers, smoother leader-follower behavior can contribute to cleaner demonstration trajectories and more consistent training data.
The B601-RS software stack is designed to integrate with the broader robot-learning workflow, including:
Teleoperation → Data Recording → Policy Training → Deployment
LeRobot integration supports both single-arm and bimanual configurations, making the platform suitable for manipulation dataset collection and physical AI experimentation.
Payload Test: Evaluating Motion Under Real Loads
Payload capacity is another important difference between a robot designed primarily for demonstration and one intended for practical manipulation.
The reBot Arm B601-RS is designed for a 2.5 kg rated payload.
To evaluate its behavior under increasing load, the arm was tested with multiple payload levels attached to the end effector while performing continuous motion trajectories across approximately 70% of its working reach.

Payload Test Results
| Payload | Observed Performance | Example Applications |
| 1 kg | Smooth continuous motion | Education, research, lightweight pick-and-place |
| 2 kg | Stable motion without visible jitter or position loss | Parts handling, lab automation, electronics |
| 2.5 kg | Stable operation at the rated payload | General manipulation and automation |
| 5 kg | Completed short-duration test motions | Temporary or experimental higher-load operation |
The 5 kg test was conducted as a short-duration validation above the rated payload, rather than a recommended continuous operating condition.
For applications requiring long-duration operation, payload selection should remain within the rated operating envelope and should also take reach, acceleration, end-effector weight, and task trajectory into consideration.
Why It Matters
A 2.5 kg rated payload expands the range of applications possible with an open-source robot arm.
Potential workloads include:
- Component and parts transfer
- Electronics handling
- Laboratory automation
- 3D printer unloading
- Vision-guided pick-and-place
- Physical AI manipulation experiments
Payload capability becomes particularly important when cameras, grippers, force sensors, or customized end effectors must also be mounted on the arm.
Repeatability Test: Maintaining Position Across Repeated Cycles
Payload determines what a robot can move.
Repeatability determines whether it can reliably return to the same location.
The reBot Arm B601-RS is specified with repeatability of ±0.1 mm.
To evaluate positioning consistency, the arm was programmed to repeatedly return to the same target position over hundreds of motion cycles, with the end-effector position monitored using a laser displacement measurement setup.

Test Result
Across repeated motion cycles, the B601-RS maintained positioning consistency within the expected repeatability range, without significant observable drift during the test period.
This is especially important for robotics applications that combine mechanical repeatability with machine vision.
A typical autonomous manipulation pipeline can include:
Object Detection → Pose Estimation → Hand-Eye Calibration → Robot Motion → Grasping
When combined with vision models such as YOLO, oriented bounding-box detection, and calibrated camera-to-robot coordinates, mechanical repeatability provides a stable foundation for more precise manipulation.
Applications That Benefit From Repeatability
Examples include:
- Camera and sensor positioning
- Electronics assembly research
- Precision dispensing experiments
- Vision-guided grasping
- Repeated laboratory workflows
- Robot learning evaluation
For Physical AI researchers, repeatability also helps reduce hardware-induced variation when comparing different policies or datasets.
Gravity Compensation: More Than a Demonstration Feature
Gravity compensation is one of the most visible capabilities of the B601-RS.
When enabled, the control system compensates for gravitational torque at each joint, allowing the arm to be repositioned manually with substantially reduced effort.
The B601-RS uses the Pinocchio rigid-body dynamics library to calculate gravitational torque and apply joint-level compensation in real time.
Two gravity-compensation modes are available, including a basic mode and an end-effector velocity-constrained mode.

Why Gravity Compensation Matters
Gravity compensation provides several practical benefits beyond manually moving the arm.
Safer Development
During debugging, calibration, and interaction with the robot, gravity compensation can reduce uncontrolled movement caused by the arm’s own weight.
Foundation for Compliant Control
Gravity compensation is an important building block for:
- Impedance control
- Force control
- Compliant manipulation
- Human-robot interaction
Removing the gravitational component from joint torque allows higher-level controllers to focus more directly on external interaction forces.
Easier Manual Teaching
For demonstration collection and manual robot teaching, reducing the physical effort required to move the arm can improve operator comfort during long data-collection sessions.
This becomes increasingly relevant as Physical AI datasets grow from dozens of demonstrations to hundreds or thousands of trajectories.
Mechanical Durability: Designed for Repeated Robotics Development
Robot development often involves more physical interaction than conventional automation.
Developers reposition arms manually, change end effectors, adjust sensors, perform calibration, recover from failed policies, and repeatedly reconfigure experimental setups.
Mechanical construction therefore becomes an important part of long-term usability.
The B601-RS introduces several structural and manufacturing improvements designed to increase rigidity, reliability, and durability.

All-Metal Structural Design
The arm uses an all-metal construction with geometric lightweighting features designed to balance structural rigidity and mass.
Load-bearing sections and joint regions have been reinforced where additional stiffness is required.
Improved Mechanical Finishing
Several smaller design details also contribute to long-term usability:
- Chamfered structural edges
- Laser-etched markings
- Metal covers for exposed fasteners
- Customized internal wiring harness
- Improved cable routing
- Reinforced load-bearing joints
These details may not directly appear in a payload specification, but they matter on a robot that will be frequently handled, reconfigured, and transported between development environments.
Actuator Robustness
The RobStride quasi-direct-drive motors used in the B601-RS provide high torque density together with overload capability suitable for dynamic robotic motion.
Combined with updated structural design and servo tuning, the B601-RS has also been optimized to reduce vibration compared with the previous reBot actuator configuration.
For robot-learning applications, lower vibration benefits not only mechanical stability but also onboard sensing and camera-based perception.
From Robot Arm to Physical AI Development Platform
The purpose of these tests is not simply to determine how much weight the B601-RS can lift.
The broader objective is to validate whether an open-source robot arm can provide the combination of mechanical performance, control responsiveness, repeatability, and software accessibility required for modern robotics development.
The B601-RS is designed for several groups of developers.
Physical AI and Robot Learning Researchers
Low-latency teleoperation, LeRobot integration, and support for data collection make the platform suitable for imitation learning and manipulation-policy research.
Universities and Research Laboratories
Its combination of payload capability, repeatability, ROS support, and open hardware makes it suitable for robotics education as well as advanced research.
Startups and Automation Developers
The 2.5 kg rated payload enables the arm to move beyond simple desktop demonstrations toward lightweight automation and prototype production workflows.
Robotics Developers and Makers
Because the platform is open source, developers can modify hardware, controllers, end effectors, and software instead of being limited to a closed ecosystem.
Why Open Source Matters
Performance is only one part of the reBot platform.
The B601-RS is designed around an open robotics ecosystem, including:
- Open-source hardware
- CERN-OHL-W 2.0 hardware license
- Full BOM
- Python SDK
- ROS 1 / ROS 2 support
- LeRobot integration
- Isaac Sim simulation platform
- Accessible motor-level control
- Customizable end effectors and accessories
This gives developers access not only to the robot’s APIs, but also to the underlying system architecture required to understand, modify, and extend the platform.
For physical AI research, this openness is particularly important.
Robot learning is evolving rapidly, and researchers increasingly need hardware that can evolve alongside new models, control methods, sensors, and training frameworks.
reBot Arm B601-RS Specifications
| Specification | reBot Arm B601-RS |
| Rated Payload | 2.5 kg |
| Repeatability | ±0.1 mm |
| Degrees of Freedom | 6+1 |
| Control Update Rate | 125 Hz |
| Communication | CAN bus, 1 Mbps |
| Actuators | 4 × RobStride RS-00 + 3 × RS-06 |
| Control | MIT control / impedance control support |
| Software | Python SDK, ROS 1/2, LeRobot,MuJoCo, Pinocchio,Isaac Sim simulation platform |
| Hardware License | CERN-OHL-W 2.0 |
Building Reliable Hardware for Physical AI
As Physical AI moves from simulation into the physical world, robot hardware needs to meet a different set of requirements.
Payload and repeatability still matter, but so do teleoperation responsiveness, compliance, maintainability, software openness, and the ability to withstand repeated experimentation.
The performance validation of the reBot Arm B601-RS reflects this philosophy.
Rather than positioning the arm only as a desktop robot, Seeed Studio is developing reBot as an open-source physical AI platform that developers can use across teleoperation, data collection, robot learning, autonomous manipulation, and lightweight automation.
For developers building the next generation of physical AI applications, reliable and accessible robotic hardware is where those models finally meet the real world.
Explore reBot Arm B601-RS
- reBot Arm B601-RS: Seeed Studio product page
- GitHub: reBot-DevArm
- Documentation: Seeed Studio Robotics Wiki
- LeRobot Integration: Seeed B601 Teleoperator Repository
FAQ
What is the payload of the reBot Arm B601-RS?
The reBot Arm B601-RS is designed with a rated payload of 2.5 kg. Actual allowable payload also depends on reach, end-effector weight, acceleration, and task trajectory.
What is the repeatability of the reBot Arm B601-RS?
The B601-RS is specified for ±0.1 mm repeatability, making it suitable for research, vision-guided manipulation, and lightweight automation applications.
Does the reBot Arm B601-RS support LeRobot?
Yes. The reBot ecosystem supports LeRobot-based workflows including teleoperation, demonstration recording, policy training, and deployment.
Does the B601-RS support gravity compensation?
Yes. Gravity compensation is available for manual teaching, compliant control development, and physical human-robot interaction workflows.
Is the reBot Arm B601-RS open source?
Yes. The reBot platform includes open-source hardware and software resources, with the hardware released under the CERN-OHL-W 2.0 license.