Content Push

The Seeedash app provides multiple ways to push content, so you can update Sticky’s screen from anywhere.

Text Push

Quotes & Messages

On the content push page, you can type text and push it to the device:

  • Inspirational quotes
  • Family messages
  • Shopping lists
  • Daily reminders

Push Steps

  1. Select the target device in the app
  2. Choose “Text Push”
  3. Enter or select text content
  4. Choose a display style template
  5. Tap “Push”

Image Push

AI Image Generation

Use the built-in AI image generation feature:

  1. Select “AI Generate”
  2. Enter an image description
  3. AI generates a black-and-white image optimized for e-ink display
  4. Preview and push to the device

Photo Album Push

Push photos from your phone’s album:

  1. Select “Album Push”
  2. Choose a photo from your phone
  3. The app automatically converts the image to e-ink-friendly format
  4. Preview and push

Tip: The e-ink screen displays black & white with 4 grayscale levels. High-contrast images work best.

Message Board

The message board feature lets you leave visible messages on the device screen:

  • Great for passing information between family members
  • Supports multiple messages displayed at once
  • Messages can be deleted from the device or the app

Next Steps