Unboxing & Setup

Package Contents

Open the box and you’ll find:

ItemQuantityDescription
reTerminal Sticky device× 1The main device
USB charging cable× 1For charging and PC connection
Adhesive magnetic ring× 1Stick to non-metal surfaces for magnetic mounting
Quick Start Guide× 1Printed brief instructions

Charge the Device

Before first use, we recommend fully charging the device:

  1. Connect the USB-C cable to Sticky’s bottom USB-C port
  2. Connect the other end to a USB charger (5V/1A is sufficient)
  3. While charging, the indicator light shows orange
  4. When fully charged, the indicator turns green
  5. Charging power is 1W — please be patient

Install the Magnetic Ring

If you want to use Sticky on a non-metal surface:

  1. Clean the target surface of dust and grease
  2. Peel off the protective film from the magnetic ring
  3. Stick the ring to the desired position, press firmly for 10+ seconds
  4. Wait 30 minutes for the adhesive to fully bond
  5. Attach Sticky to the magnetic ring

Tip: If the target surface is metal (like a fridge door), you can attach Sticky directly — no magnetic ring needed.

Power On

Press and hold the AI button to turn on the device. On first boot, the screen will display a pairing guide prompting you to download the mobile app and pair.

Next Steps