Power & Charging

Battery Specs

ParameterSpecification
Battery typeLithium-ion
Capacity700mAh
Charging portUSB-C
Charging power1W

How to Charge

  1. Connect the included USB-C cable to the device
  2. Connect the other end to a 5V USB charger
  3. While charging, the indicator shows orange
  4. When fully charged, the indicator turns green

Tip: Charging power is 1W. We recommend charging overnight or when the device is not in use.

Battery Life Optimization

Deep Sleep Mode

Sticky supports deep sleep mode, which significantly extends standby time. You can enable “Long Battery Life Mode” in system settings.

Wake Methods

The device can be woken from deep sleep by:

  • Touch — Touch the screen to wake
  • Button — Press any button to wake
  • Timed wake — Automatically wake at set intervals to update content

Battery Life Tips

  • Enable long battery life mode for low-frequency use scenarios
  • Reduce high-frequency content refreshes
  • Avoid frequent full-screen refreshes
  • Use partial refresh mode for content updates

Low Battery Alert

When the battery drops below the threshold, the Seeedash app will receive a low battery alert, reminding you to charge in time.

Next Steps