Wi-Fi Configuration
reTerminal Sticky connects to Wi-Fi with help from the mobile app. Once configured, the device can run independently without your phone staying connected.
Prerequisites
- Seeedash app downloaded and installed
- Phone Bluetooth enabled
- Device powered on and in pairing mode
- 2.4GHz Wi-Fi name and password ready
Note: Sticky only supports 2.4GHz Wi-Fi, not 5GHz networks.
Setup Steps
1. Open Seeedash App
Launch the Seeedash app on your phone and go to the device management page.
2. Add New Device
Tap the “Add Device” button. The app will automatically scan for nearby Sticky devices via Bluetooth.
3. Select Device
From the scanned device list, select your Sticky device to pair.
4. Enter Wi-Fi Info
Enter your 2.4GHz Wi-Fi name and password in the app. The app will send the network info to the device via Bluetooth.
5. Wait for Connection
After receiving the Wi-Fi info, the device will automatically try to connect. Once connected, the screen will update with content.
Common Issues
Connection failed?
- Confirm the Wi-Fi is 2.4GHz
- Confirm the Wi-Fi password is correct
- Make sure the device isn’t too far from the router
- Try restarting the device and reconfiguring
How to change Wi-Fi?
In Seeedash app’s device settings, select “Change Network” and follow the prompts to reconfigure.
Next Steps
- First Use Tutorial — Learn basic operations