Seeed Studio Unveils SenseCAP S700-C: Bringing Industrial-Grade Radar Weather Sensing to the Mass IoT Market

By replacing fragile mechanical components with solid-state radar and ultrasonic technology, the SenseCAP S700-C weather station offers uninterrupted rain, snow, hail, and wind monitoring in the world’s harshest environments.

product photo of  the S700-C weather station

Düsseldorf, Germany — For decades, deploying a remote weather station has meant accepting a painful compromise: high maintenance costs or frequent data gaps. Traditional mechanical sensors—such as tipping-bucket rain gauges and cup-and-vane wind meters—are prone to fail in long-term deployments. They freeze in winter, clog with leaves in autumn, and wear out from constant friction.

To break this cycle of high maintenance and unreliable data, Seeed Studio has launched the SenseCAP S700-C, an industrial-grade, all-in-one compact weather station. By engineering a 100% solid-state architecture with zero moving parts, the S700-C redefines what is possible in remote environmental monitoring.

The Three Tech Breakthroughs of the SenseCAP S700-C

  1. Doppler Radar Sensing Technology

Unlike traditional tipping buckets that only measure liquid rainfall, the S700-C features a high-precision 60GHz Radar sensor.

  • The Advantage: It measures the size and velocity of falling droplets, allowing it to accurately detect, distinguish, and measure rain, snow, and hail.
  • The Impact: Since there is no physical funnel to clog, the sensor requires zero cleaning or maintenance, ensuring continuous data flow during autumn leaf drops or winter blizzards.
  1. Ultrasonic Wind Measurement

Mechanical wind cups requires a certain amount of wind to start monitoring, and they wear out over time, leading to friction and inaccurate low-wind readings.

  • The Advantage: The S700-C utilizes ultrasonic sound waves to calculate wind speed and direction with no physical wear.
  • The Impact: It maintains factory-level calibration and accuracy over years of operation, eliminating the need for regular field recalibration.
  1. 7-in-1 Industrial Integration meeting IP66 Standards

Instead of purchasing, wiring, and mounting multiple separate sensors, the S700-C integrates 7 critical parameters into a single, sleek, highly ruggedized unit:

  • Air Temperature, Relative Humidity, Barometric Pressure, Light Intensity, Precipitation/Snow/Hail, Wind Speed, and Wind Direction.
  • The Impact: It reduces installation time from hours to minutes and lowers the total cost of ownership (TCO) for large-scale IoT deployments.

Designed for the “Unreachable” Locations

“When you are deploying weather sensors on top of a mountain for landslide warning, or in the middle of a 1,000-acre smart orchard, sending a technician to fix a stuck wind vane is a logistical nightmare,” said Jenkin, Product Manager at Seeed Studio. “We built the SenseCAP S700-C for the ‘unreachable’ spots. It is a true ‘set-and-forget’ system designed to deliver high-fidelity data under the most brutal outdoor conditions.”

Deploy-and-Forget in Agriculture: The fully solid-state Seeed Studio SenseCAP S700-C, installed in a smart farm, provides uninterrupted micro-climate data. Its radar-based sensor can detect hail early, allowing growers to deploy crop-protective netting just in time.

(Deploy-and-Forget in Agriculture: The fully solid-state Seeed Studio SenseCAP S700-C, installed in a smart farm, provides uninterrupted micro-climate data. Its radar-based sensor can detect hail early, allowing growers to deploy crop-protective netting just in time. )

Enhanced Hydrological Safety: The SenseCAP S700-C is deployed alongside a critical watershed to monitor flash flood and landslide risks. Its ability to measure liquid rainfall as well as snow ensures more accurate predictive water modeling for smart city disaster prevention.

(Enhanced Hydrological Safety: The SenseCAP S700-C is deployed alongside a critical watershed to monitor flash flood and landslide risks. Its ability to measure liquid rainfall as well as snow ensures more accurate predictive water modeling for smart city disaster prevention.)

Optimized for Mass IoT Integration

The SenseCAP S700-C is fully compatible with standard industrial communication protocols, including RS485 (Modbus-RTU) and SDI-12, fully interoperable with existing data loggers and industrial systems. Besides, Seeed also offers a plug-and-play seamless integration experience with SenseCAP Sensor Hub 4G Data Logger and SenseCAP S2100 LoRaWAN DTU for quick configuration and deployment.

Availability for Global Mass Deployment

The SenseCAP S700-C is now available for order worldwide via the Seeed Studio Official Store and authorized global distributors. For bulk inquiries or custom industrial integrations, please contact our sales team at seeed_emea[at]seeed[dot]cc.

About Seeed Studio

Seeed Studio is an open-hardware company headquartered in Shenzhen, China, with branch offices in Germany, Japan, and the United States. Specialized in Edge AI and IoT, Seeed offers a full stack of products—from smart sensor networks to edge AI computers—along with customization services for global developers, independent software vendors (ISVs), and system integrators since 2008. With an in-house wind-tunnel laboratory, Seeed strictly ensures that its weather sensors are tested, calibrated, and validated for performance.

Seeed’s products and services are widely deployed in solutions for smart cities, smart agriculture, smart retail, smart manufacturing, and more.

About Author

Calendar

May 2026
M T W T F S S
 123
45678910
11121314151617
18192021222324
25262728293031