Wireless Security Testing with XIAO ESP32-C5: A Guide to Dual-Band Wi-Fi 6 & IoT Auditing

Explore real-world wireless security case studies using the XIAO ESP32-C5. See how researchers deploy this dual-band Wi-Fi 6 chip for wardriving and audits.

In our previous article, we explored the raw wireless performance of the XIAO ESP32-C5 and its potential across wireless security and smart home ecosystems. As a budget-friendly, dual-band Wi-Fi 6 microcontroller, it successfully fills the 5GHz gap that previously limited independent hardware research. Today, we are moving from theory to execution to showcase a definitive real-world case study of the XIAO ESP32-C5 in action within the cybersecurity space.

The Evolution of Pocket-Sized Pentesting

For years, popular wireless security tools such as ESP8266 Deauther, ESP32 Marauder, Flipper Zero, HackRF One, Cardputter, and various DIY Wi-Fi auditing devices have been staples in the toolkit of security researchers. However, as the world moves to 5GHz highways and Wi-Fi 6 (802.11ax) protocols, these legacy tools are left blind. Security researchers are severely bottlenecked by 2.4GHz constraints and outdated Wi-Fi 4 hardware.
 
Enter the Seeed Studio XIAO ESP32-C5. This thumb-sized powerhouse is the first RISC-V SoC from Espressif to combine dual-band Wi-Fi 6, Bluetooth 5, and 802.15.4 (Zigbee/Thread) in a microscopic form factor. While most ESP32 Wi-Fi tools, scanners, analyzers, and Marauder-based projects remain limited to 2.4GHz operation, the XIAO ESP32-C5 introduces native 5GHz Wi-Fi support in a board smaller than many popular portable hacking tools. For users exploring ESP32 Marauder, Flipper Zero Wi-Fi expansions, and next-generation wireless research platforms, it opens new possibilities for building ultra-compact dual-band Wi-Fi devices.

🛡️ Why XIAO ESP32-C5 Is Ideal for Next-Generation Hacking Tools?

Dual-Band Dominance: Over 70% of modern enterprise networks run on 5GHz. The XIAO ESP32-C5 unlocks this spectrum for budget hardware, enabling researchers to perform passive reconnaissance where older chips failed.
Wi-Fi 6 & WPA3 Validation: Test how modern routers handle transition modes, management frame protection, and efficiency features like Target Wake Time (TWT).
Multi-Protocol Concurrency: Audit the security of smart hubs by interacting with Wi-Fi backhauls and Zigbee/Thread sensor networks simultaneously.

📋 Currently Supported Firmware:

GhostESP: Provides a polished, mobile-friendly web interface that serves as a portable wireless audit “Swiss Army Knife.”

Bruce Firmware & ESP32 Marauder is waiting for support…

🛠️ Hardware Setup & Recommendations

To get the most out of your security testing, we recommend the following hardware layout:

🔍 Practical Security Testing Case

[ Case 1 ] The "Piglet" Project — DIY ESP32 Wardriver

💡What It Is:

The “Piglet” is an open-source, DIY pocket-sized rig built specifically for dual-band ESP32 wardriving (a device used to map and log the locations of wireless networks). 

Designed by Hamspice from Midwest Gadgets, it enables enthusiasts to solder together a custom PCB to create a powerful dual-band wifi scanner. By combining the robust ESP32 Wi-Fi capabilities of the Seeed Studio XIAO ESP32-C5 with accurate GPS tracking, it logs wireless networks while on the move. Crucially for modern wifi security auditing, its 5GHz reach captures networks that legacy 2.4GHz tools—like a standard ESP32 marauder or a stock flipper zero—often miss entirely.

🛠️How It Works:

  • Dual-Band Recon & GPS Sync: Operating as a passive Wi-Fi scanner, the core MCU (XIAO ESP32-C5) continuously catches Wi-Fi beacon frames across both 2.4GHz and 5GHz frequencies. Simultaneously, the onboard high-accuracy ATGM336H GPS module locks onto satellites to get precise geographical coordinates.

  • Log Logging (The Payload): The ESP32 Wi-Fi module pairs the captured network intelligence (SSID, MAC address, signal strength) with the exact GPS coordinates and time stamps, continuously writing this ESP32 wardriving tracking data onto an SPI SD Card module.

  • User Interaction: A 0.96-inch OLED display shows live system stats, randomized start-up animations, and GPS status (blinking when locked). A single physical tactile switch button allows the user to cycle through different UI screens or toggle the display on/off to save battery.

[ Case 2 ] Portable Real-Time Wireless & Bluetooth Attack Detector

💡What It Is:
A DIY smart nightlight that doubles as a real-time wireless security detector. Disguised as a standard ambient lamp, it actively functions as an ever-watchful Wi-Fi scanner, sniffing out Wi-Fi disconnect attacks (Deauth floods) and Bluetooth pop-up spam often launched by pranksters using a Flipper Zero or an ESP32 marauder. While mobile ESP32 wardriving rigs are built to map networks on the go, this stationary sentinel is designed to protect your personal space.
 
🛠️How It Works:
  • The Tech: It combines a tiny ESP32 microcontroller with a 6×10 RGB LED matrix inside a 3D-printed case.

  • The Defenses: The chip constantly monitors the airwaves. If it detects a wireless attack, the nightlight flashes a red warning.

  • The Controls: It hosts its own local Wi-Fi network. You connect with your phone to change the light modes (fade, wave, flicker) or read the security attack logs.

When it detects Bluetooth spam, a sudden surge of nearby Bluetooth devices, or someone entering the house, the device starts flashing as an alert.

[ Case 3 ] Single-Chip Dual-Band Wi-Fi Scanner

💡What It Is:

This is a portable Wi-Fi analyzer and spectrum detector. It scans surrounding wireless signals in real time and graphically displays channel utilization and signal strength across both 2.4GHz and 5GHz bands on a connected screen. Users can carry it anywhere to assess local network congestion, making it easy to select the cleanest, lowest-interference channel for their own wireless routers.

🛠️How It Works:

  • RF Scan: The ESP32-C5 continuously hops through all 2.4GHz and 5GHz channels to catch Wi-Fi beacon frames.

  • Data Extraction: For every network found, it grabs two raw values: Channel Number (where it is) and RSSI (how strong it is).

  • Coordinate Mapping: The code converts these values into screen coordinates: X-axis = Channel, Y-axis = Signal Strength.

  • Parabolic Render: It draws each network as a parabolic curve on the screen. Overlapping curves instantly show you which channels are congested.

[ Case 4 ] The "BIS Combobulator" — A Multi-Channel ESP32 Wardriving Cluster

💡What It Is:

The “BIS Combobulator” is a DIY, high-performance hardware cluster tool designed for ESP32 Wardriving (wireless network mapping) and Red Team cybersecurity testing.

Built by tech makers Cal and Zeke, it pairs multiple Seeed Studio XIAO ESP32-C5 microcontrollers inside a 3D-printed, weatherproof enclosure equipped with heavy-duty magnets for vehicle mounting. Running on the Biscuit Manager app ecosystem, this portable “device army” leverages the dual-band Wi-Fi 6 capabilities of the ESP32-C5 to intercept, map, or stress-test wireless networks on a massive scale.

🛠️How It Works:

  • Parallel Scanning: Instead of one chip scanning everything, the workload is split. Individual ESP32-C5 nodes are assigned to lock onto and monitor separate, specific channels simultaneously.

  • Dual-Mode Execution:

    • War Driving: The nodes capture overlapping signals at high speeds, logging up to 150 networks per foot while driving.

    • Red Team Testing: The cluster coordinates to send simultaneous Deauthentication (Deauth) frames, instantly disconnecting multiple target devices across 2.4GHz and 5GHz bands.

  • Simple Parallel Power: Due to the low power draw of the C5 chips, the entire cluster runs on a basic 6-way USB splitter powered by a single 6,000 mAh battery, lasting up to 6 hours.

The Next Evolution: Moving to an ESP32-C5 Marauder Setup

Let’s be real—if you are into hardware hacking, you probably already have a standard ESP32 marauder sitting on your desk or plugged into your Flipper Zero. It’s a legendary tool, but it has one massive blind spot: it’s entirely deaf to 5GHz networks.

That’s exactly why the community is shifting toward the ESP32-C5 marauder concept. By pairing the familiar Marauder workflow with the dual-band Wi-Fi 6 capabilities of the XIAO ESP32-C5, you stop missing half the traffic in the air. Whether you’re building a standalone pocket Wi-fi scanner or a dedicated ESP32-C5 marauder companion module, this silicon upgrade is quickly becoming the new baseline for authentic Wi-Fi security auditing.

🛡️ Mitigation, Compliance & Ethics

Defensive Perspective: Securing Networks Against Low-Cost Dual-Band Auditing
The accessibility of boards like the XIAO ESP32-C5 proves that dual-band and Wi-Fi 6 threats no longer require expensive laptop rigs or high-end external Wi-Fi cards. To secure your infrastructure:
  1. Enforce Strict WPA3-Only Mode: Eliminate WPA2 Transition Modes to prevent downgrade vulnerabilities.
  2. Mandate PMF (Protected Management Frames): Ensure management frames are encrypted to mitigate unauthorized disassociation risks.
  3. Isolate IoT Infrastructure: Place Zigbee/Thread gateways and Wi-Fi 6 IoT devices on strict, monitored VLANs away from corporate data.
Legal & Ethical Compliance Disclaimer
Important Note: This guide is strictly intended for educational purposes, authorized penetration testing, and academic wireless security research. Intercepting or auditing wireless networks without explicit, written permission from the network owner is illegal and violates privacy laws. Always ensure you are testing within a controlled laboratory environment or an authorized scope of work.

End Note

Hey community, we’re curating a monthly newsletter centering around the beloved Seeed Studio XIAO. If you want to stay up-to-date with:

🤖️ Cool Projects from the Community to get inspiration and tutorials
📰 Product Updates: firmware update, new product spoiler
📖 Wiki Updates: new wikis + wiki contribution
📣 News: events, contests, and other community stuff

Please click the image below👇 to subscribe now!

About Author

Calendar

May 2026
M T W T F S S
 123
45678910
11121314151617
18192021222324
25262728293031