Now You Can Turn Sticky into Your Personal Dashboards with TRMNL BYOD

Meet Sticky × TRMNL: our compact magnetic ePaper display now runs the TRMNL dashboard ecosystem. Customize plugins for calendars, flights, parcels & more.

reTerminal Sticky (available for pre-order with shipment on November 20, 2026) was designed to bring information you care about into your everyday spaces. With its compact 3.97″ magnetic ePaper display, low-power design, and flexible placement, Sticky makes it easy to keep important information visible, whether on your fridge, desk, wall, or workspace.

But the possibilities of such a tiny magnetic ePaper display do not stop there.

We’re super excited to share that our collaboration with the amazing TRMNL team has found its new presence in our latest ePaper display Sticky. Since our joint effort in launching the TRMNL 7.5″ (OG) DIY Kit last year, we’re now bringing the TRMNL open-source ePaper dashboard ecosystem to Sticky’s compact magnetic design. With TRMNL BYOD architecture, Sticky can now connect to a growing ecosystem of dashboards, plugins, and integrations. From calendars and flight information to movie watchlists, parcel tracking, smart home data, and more, Sticky becomes a customizable low-distraction display built around your needs, keeping them visible in your daily routine.

TRMNL on reRerminal Sticky

Spoiler. To celebrate this collaboration, the TRMNL team is offering an exclusive offer for the TRMNL BYOD access. Limited to the first 200 licenses, one per customer. Read on to seize the opportunity to save BIG on the TRMNL BYOD license.

What Does TRMNL Bring to Your Sticky?

With more than 1,300 plugins available in its Integration Library, TRMNL connects the tools and services you already use. It adds rotating playlists, external plugins, and flexible mashup layouts, turning Sticky into a dynamic information display that adapts to your needs.

We're (TRMNL) thrilled to add compatibility to Seeed's latest gadget Sticky, which is priced extremely competitively and full of unique features. My own Sticky is currently showing me short stories in the language I'm studying, and I take it with me to cafes whenever I work remotely. Adding a BYOD license to your Sticky will give it instant access to over 1,300 plugins and a 9,000+ person developer community on Discord for even more fun and tinkering.
Ryan Kulp
Founder of TRMNL

Here are some more ideas to inspire your next Sticky setup:

  • Upcoming Movies / Letterboxd

Keep track of movies you want to watch and your personal viewing activity.

  • Parcel Tracking

Stay updated on deliveries without constantly checking your phone.

  • Flight Tracker / Trainboard

Display travel information and transportation updates at a glance.

  • Notion

Bring your notes, to-do lists, and project updates to your Sticky display.

  • ISS Location

Follow the International Space Station’s current position from your desk or wall.

  • Smart Home Dashboards

Energy, climate from Homey or entity cards, to-do list, sensor data from Home Assistant

Whether you use Sticky as a productivity tool, travel companion, a portable home panel, or just a fun information display, TRMNL gives you more ways to make it your own.

The Special TRMNL BYOD Offer

To celebrate this new collaboration, we’re partnering with the TRMNL team to offer the TRMNL BYOD license at an exclusive price of just $35, with a 30% off (normally $50). Just use code “trmnl-sticky” at checkout. Limited to the first 200 accesses, one per customer. Don’t miss out!

TRMNL BYOD (Bring Your Own Device) is a one-time license that gives compatible ePaper devices access to the TRMNL web application, private plugin API, and one connected device. With BYOD access, you can unlock the full TRMNL experience and start building customized ePaper dashboards with your favorite plugins, layouts, and integrations.

BTW, if you also own our reTerminal ePaper displays (reTerminal E1001, E1002, E1003 and E1004), which are all TRMNL-compatible, you can enable the TRMNL BYOD license you got on these displays as well. One license, perpetual use for 1x device. You can explore more cool use cases the community is building using reTerminal ePaper displays together with TRMNL BYOD.

How to Get Started with TRMNL BYOD on Sticky

Step 1

Get a Sticky. Then flash the TRMNL firmware to Sticky in either Sticky Playground or the official TRMNL Flasher (V1.8.17 is recommended)

Step 3

Visit your device settings page to select your Device Model and then, under the Developer Perks section set your device’s MAC address. By now, you’ve added the Sticky to your TRMNL BYOD account.

Step 4

Choose your plugins and build your playlist.

For the complete Flash guide, visit here to get started quickly.

One Sticky, More Ways to Use It

Last but not least, for those who might not be familiar with Sticky yet, Sticky is an ESP32-S3-based open hardware platform, that works with different software ecosystems, including the amazing TRMNL, ESPHome & OpenDisplay for Home Assistant, CrossPoint eReader, the SenseCraft Seeedash mobile app, and other community-created firmware.

Whether you want to build a family information board, a smart home control panel, a productivity companion, a portable e-reader, or even something completely unexpected, Sticky gives you the freedom to create. Sticky is now available in instant stock, and please do seize the chance to grab one while the stock lasts. 🙂

Thanks for sticking with us.

Last but not least, if you’d love to get more first-hand updates on reTerminal Sticky, you’re invited to join our growing Sticky Facebook Group, where the whole community is showcasing their cool and unique builds with Sticky.

About Author

Leave a Reply

Your email address will not be published. Required fields are marked *

Calendar

November 2026
M T W T F S S
 1
2345678
9101112131415
16171819202122
23242526272829
30