Monthly Wrap-Up for June 2026 New Hardware, Robotics Solutions, PCBA Guides & Community Creations

Hey community,

Welcome to the latest edition of Seeed Monthly! This month, we bring you 5 in-depth technical articles with professional insights, 5 stunning product and service showcases, 6 latest Seeed updates and event highlights, as well as 5 inspiring open-source community projects. Let’s dive right in!

📚 I. In-depth Feature & Tech Exploration

Machine learning lets computers learn from data and make decisions or predictions without being explicitly programmed. It’s applicable in various industries, from improving healthcare with predictive diagnostics to detecting pollution to protect the environment, optimizing retail supply chains, and advancing autonomous vehicle technology. Machine learning helps to enhance our lives, and with compact machine learning modules, it’s become accessible for everyone to explore and innovate in our daily routines.

01. Seeed Jetson DevelopTool Overview

Seeed Jetson DevelopTool is an all-in-one AI development workbench designed for Seeed Studio Jetson products. It consolidates the most common Jetson development workflows — from first-time firmware flashing to AI app deployment — into a single desktop GUI application. Check Out today.

02. reCamera Pro Quick Start Guide

pir

This guide will assist you in completing the hardware connection, logging into the device Web interface, configuring the wireless network, and troubleshooting common connection failures. Find more details here.

03. Getting Started with Seeed Studio XIAO nRF54LM20A Sense

pir

Seeed Studio XIAO nRF54LM20A Sense is a compact, ultra-low-power wireless development board built around Nordic Semiconductor’s nRF54LM20A SoC. It combines a 128 MHz Arm Cortex-M33 processor, 512 KB RAM, 2 MB on-chip NVM, multiprotocol 2.4 GHz wireless connectivity, onboard IMU, digital microphone, 8MB external flash, IPEX antenna connector, and nPM1300 PMIC for advanced battery-powered IoT, wearable, smart sensing, and edge AI applications. Check out today.

04. reBot Arm B601-DM GraspNet Visual Grasping on Jetson

The demo combines an RGB-D camera, YOLO instance segmentation, GraspNet 6-DoF grasp pose estimation, eye-in-hand calibration, and real robot control, so the arm can select and grasp common objects on a table.

Click for more.

05. reComputer Mini J501 WiFi Module Installation

In this document, you will learn how to disassemble the reComputer Mini J501 and install or replace a Wi-Fi module (M.2 Key E). Check out today.

📰 II. Product & Service Showcases

Stay up-to-date with the latest product releases from Seeed. Discover new tools, platforms, and services designed to streamline your workflow and accelerate innovation in your projects.

01. NVIDIA Jetson Thor + reBot Arm Voice Control Robotic Arm Tutorial

We just published a complete tutorial showing how to deploy an end-to-end voice-controlled grasping system for the reBot Arm B601, running entirely on the NVIDIA Jetson Thor platform. Find out more here.

02. reBot Arm Debuts at ICRA 2026, Showcased by Foxglove

Seeed Studio’s reBot arm will be exhibited at Foxglove Booth 70 during ICRA 2026. Thanks to Foxglove’s Robotics Developer Relations Mateusz Sadowski, the 6+1 DoF reBot (1.5kg payload, 767mm reach, 0.2mm repeatability, starting at $1,200 pre-assembled) will demonstrate camera payload carrying, Python SDK control, URDF state visualization, joint data monitoring and real-time point cloud rendering via Foxglove’s multimodal robot data platform. Read more.

03. Sharing of reBot Arm + GraspNet + VLA Robotic Grasping Solution

The project integrates VLA to advance zero-shot end-to-end robotic learning. The team also deployed GraspNet-Baseline to conduct 6D grasping pose estimation from RGB-D point clouds, leveraging YOLO bounding boxes and OBB models to extract target objects for complex grasping tests. Read more.

04. Pre-sale Warm-up for reSpeaker Clip AI Audio Recorder

The reSpeaker Clip AI recorder is coming soon for pre-order. Designed for all-day, privacy-focused AI recording, it features 2GB local storage supporting up to 256 hours of offline recording to secure your data. It delivers long-lasting battery performance: 18 hours in endurance mode and 14 hours with noise suppression enabled for meetings and daily voice capture. Read more.

05. Introduction to Gravity Compensation Function of reBot Arm B601-RS

The reBot Arm B601-RS integrates built-in gravity compensation to counteract self-weight interference, delivering steady, smooth and predictable robotic movement. It cuts motor debugging workload, ensures consistent motion performance and accelerates project rollout, allowing developers to concentrate on AI vision and upper-layer application development rather than mechanical parameter tuning. Read more.

👩‍💻 III. News & Event Highlights

Get the inside scoop on recent events and news. Gain valuable insights, key takeaways, and highlights from industry experts and thought leaders at the forefront of ML innovation.

01. XIAO nRF54LM20A (Sense) – Ultra-Low Power Multi-Protocol IoT Board with Motion Wake-Up

Seeed launches XIAO nRF54LM20A and its Sense variant based on Nordic nRF54LM20A SoC and nPM1300 PMIC, following official Nordic EVB standards for superior low-power performance. It supports BLE 6.0, Matter, Thread and Zigbee, equipped with large memory, 28 GPIOs and onboard NFC. The Sense model adds a 6-axis motion wake-up IMU and digital mic. Optimized RGB LEDs cut standby power to zero, and shiphold mode avoids battery leakage during storage. More info.

02. ESP32-C5 vs ESP32-C6: Why It’s a Great Choice for Modern Home Assistant Projects

ESP32-C5 Home Assistant

While ESP32-C6 dominates smart home projects with a mature Home Assistant and ESPHome ecosystem, the ESP32-C5 stands out with exclusive 5GHz dual-band Wi-Fi and a faster 240MHz single-core processor. Fully compatible with ESPHome, Matter, Thread and Zigbee protocols, it effectively avoids 2.4GHz network congestion, delivers more stable and high-throughput connections. Ideal for smart displays, dashboards and data-intensive smart home devices, ESP32-C5 serves as a perfect complementary solution for advanced and complex smart home deployments. More info.

03.From Bare Board to Working PCBA: 6 Key Steps That Bring Electronics to Life

Standard PCBA manufacturing transforms blank PCBs into fully functional boards via six core processes: solder paste printing, precise SMT component placement, temperature-calibrated reflow soldering, THT component insertion, wave soldering, and final functional testing. Strict control of every step eliminates soldering flaws and functional risks, ensuring stable, reliable and mass-production-ready circuit boards. Find out more.
 

04.From Standard Device to Branded Product: A Seeed Fusion Light Customization Case Study

Seeed Fusion delivered a lightweight white-label customization service for a European client. Based on standard off-the-shelf hardware, we completed brand logo silk-screen printing, exclusive packaging design and sample validation. After successful small-batch trial production, the customer quickly scaled up to a 500-unit repeat order. With finalized artwork and production settings, follow-up orders require no extra NRE cost, enabling low-threshold, fast brand iteration and flexible mass production for hardware white-label projects.

More info.

05.Introducing the XIAO Project Hub: Discover What You Can Build with XIAO

XIAO Project Hub

Countless innovative projects based on thumb-sized XIAO boards were previously scattered across various platforms. To unify these resources, Seeed officially launched the open XIAO Project Hub on GitHub. It centrally collects and categorizes massive community creations, supporting flexible filtering by project category, board model, release time and more. Built for makers, the open and continuously updated platform allows users to easily explore inspirations, find practical projects and submit their own works to enrich the XIAO hardware ecosystem.

Find out more.

 

06.PCBA File Preparation Checklist: What to Prepare Before Production

Complete and consistent production files are the prerequisite for efficient PCBA manufacturing. Standard file packages including Gerber, BOM, CPL, assembly drawings, schematics and complete test documents ensure accurate quotation, component sourcing, SMT placement, soldering and functional testing. Uniform file versions avoid repeated confirmation, placement errors and testing risks. Clear test standards and firmware version specifications further reduce defects and rework costs, enabling smooth DFM review and mass production delivery.

Register Now.

🌈 IV. Community Project Spotlight

Celebrate the creativity and ingenuity of our community members with featured projects and ideas in machine learning. From open-source libraries to DIY solutions, there’s no shortage of inspiration to be found among our talented community.

01. XIAO EE05 Home Assistant Air Quality ePaper Dashboard Project

Maker Ernesto Tolocka created a persistent air quality ePaper dashboard based on XIAO EE05 ESP32-S3 Plus and a 4.26-inch monochrome 800×480 e-ink screen. It retrieves real-time temperature, humidity, CO₂, formaldehyde and VOC data from Home Assistant via REST API. Thanks to ePaper’s ultra-low power trait that retains content without power and performs well under bright light, the device connects to Wi-Fi, refreshes readings and enters deep sleep automatically, offering a dedicated physical screen for intuitive smart home air quality monitoring. Check it out . 

02. XIAO ESP32-C5 Dual-MCU 5GHz Wi-Fi Project

查看图片

Maker Zeller MA developed a dual-MCU solution with two XIAO ESP32-C5 boards. One runs esp-at firmware as an independent 5GHz Wi-Fi communication module connected via UART, and the other serves as the main controller to drive an ILI9341 SPI screen. Separating wireless and main control reduces single-chip load, ensures smooth main program operation, and supports replaceable communication modules. The compact XIAO form factor enables this multi-MCU design implemented on custom PCBA, which refreshes the display and outputs real-time Wi-Fi status through AT commands. Learn more.

03. Recruitment of Global Workshop Partners for Seeed Physical AI

查看图片

Seeed is recruiting global workshop partners in two tracks: city co-hosts with venues and event resources, and Physical AI pioneer ambassadors including developers and creators. Partners get robot hardware kits, full technical materials, global co-brand promotion and engineering support. We have partnered with NVIDIA Robotics, Hugging Face and more to hold worldwide tech events. Find out more.

04. XIAO ESP32-C5 BLE & Wi-Fi Signal Radar Scanner Project

Maker Notorious Squirrel built a portable BLE/Wi-Fi signal radar scanner with XIAO ESP32-C5 and XIAO round touchscreen. It calibrates ambient signal baseline on startup, alerts users of new nearby devices via animated radar view, supports 2.4G/5G dual-band scanning and mode switching, and stores detection logs on SD card. Check it out . 

05. XIAO ESP32-C6 Vintage ePaper Weather Station Project

Maker Dan King created the retro-style Veltoc Model 01 weather station based on XIAO ESP32-C6, equipped with a 2.9-inch ePaper screen and BME280 sensor to display temperature, humidity, air pressure and time. It features a rotary knob for page switching, 3D printed shell and 1400mAh battery supporting 3–6 months of use due to ultra-low power ePaper. Check it out . 

That’s all for today, thank you all for reading through this June Monthly Wrap-up in your spare time. (It is indeed a fruitful month!) If you wanna share what projects you’re working on, shoot us a tweet @seeedstudio, let us know on LinkedIn and Discord, or publish your project on our Project Hub on Hackster.

 

 

#Notes

If you’re new to this session, here is a brief intro. We have gotten dozens of requests over the years for a Seeed Monthly Newsletter. Although we already have a newsletter for weekly updates, we still need a place to host overall information about what’s happened on a monthly basis. It can offer an efficient and friendly way to get updated for the whole community. And that’s what we expect for our Seeed Monthly Wrap-ups. Instead of putting it as a subscribe-to-read format, we’re publishing them on our blog, so as to keep it as open and accessible as possible for the whole community. For each entry, we will cover awesome projects from the community, campaigns that we are running, new products, IIoT Solutions, and even secret recipes for prototyping and manufacturing.

 

About Author

Calendar

July 2026
M T W T F S S
 12345
6789101112
13141516171819
20212223242526
2728293031