Seeed Studio at Meteorological Technology World Expo 2026
Seeed Studio will join Meteorological Technology World Expo 2026 in Amsterdam, bringing a broad portfolio of compact weather sensors, connected environmental monitoring devices, data loggers, and selected field sensors to the global meteorological technology community.
Visit us at Booth H33 to see how precise multi-parameter sensing can move from outdoor measurement to reliable data access for agriculture, smart cities, renewable energy, hydrology, and other demanding environments.

What Is Meteorological Technology World Expo 2026
Meteorological Technology World Expo is an international exhibition for meteorological, hydrometeorological, metocean, and environmental monitoring technologies and services.
The 2026 edition will take place at RAI Amsterdam from 6 to 8 October, bringing together more than 150 solution providers and professionals from more than 80 countries. The event is organized by CloserStill Media and UKi Media & Events, the organizations behind the Meteorological Technology International media platform.
The 2026 Expo will be organized in parallel with the World Meteorological Organization Technical Conference on Instruments and Methods of Observation (WMO TECO-2026). The conference will run from 5 to 8 October under the theme “Developments in Earth System Measurements and Technologies.”
This connection places the exhibition within a wider program focused on the measurement methods, instruments, and technologies that support weather and Earth system observation.

Seeed Studio at Booth H33
Seeed Studio will attend as a professional weather sensor provider and environmental monitoring technology company.
At Booth H33, we will present the SenseCAP ecosystem as an end-to-end approach to field intelligence: select the measurements required by a site, connect them through LoRaWAN, 4G, or wired industrial interfaces, and route the resulting data to SenseCraft, an open API, or a customer’s own platform.
The showcase will cover the SenseCAP all-in-One family of compact weather sensors, the SenseCAP S2120 LoRaWAN weather station, the SenseCAP Combo 5-in-1 Sensor with 4G, data logger options, and selected SenseCAP LoRaWAN environmental and RS485 environmental sensors.
Together, these products cover different measurement depths, installation constraints, connectivity requirements, and deployment scales.
Products on Display
The products below represent the planned showcase. Product availability and the final physical display may be adjusted before the event, but the portfolio illustrates the range of sensing and connectivity options visitors can discuss with the Seeed team.
| Product | Category | One-sentence introduction |
| SenseCAP S200 | Ultrasonic wind sensor | A focused wind measurement option for projects that need reliable wind speed and direction data without deploying a full multi-parameter station. |
| SenseCAP S600-A | 6-in-1 compact weather station | Adds light intensity to the core temperature, humidity, pressure, and ultrasonic wind measurements for outdoor and agricultural monitoring. |
| SenseCAP S700 | 7-in-1 compact weather sensor | A versatile professional station for core atmospheric measurements, with variants that support different rainfall and solar radiation requirements. |
| SenseCAP S700-A | Radar rain variant | Combines the S700 platform with radar-based rainfall measurement for responsive precipitation monitoring with low mechanical maintenance. |
| SenseCAP S700-B | Solar radiation variant | Adds solar radiation measurement for applications such as solar resource assessment, agriculture, and environmental research. |
| SenseCAP S700-C | Solar radiation and radar rain variant | Integrates pyranometer-based solar radiation and radar rainfall sensing, with precise wind measurement for demanding field deployments. |
| SenseCAP S800 | 8-in-1 compact weather sensor | Combines atmospheric measurements with PM2.5, PM10, and noise monitoring for smart city, transport, agriculture, and environmental applications. |
| SenseCAP S1000 V2 | 10-in-1 compact weather sensor | Brings together temperature, humidity, pressure, light, optical rainfall, ultrasonic wind, PM2.5, PM10, and CO2 in one rugged station. |
| SenseCAP S2120 | 8-in-1 LoRaWAN weather station | A wireless outdoor station for transmitting temperature, humidity, pressure, light, rainfall, wind speed, wind direction, and related weather data over LoRaWAN. |
Connected Monitoring and Data Collection
| Product | Category | One-sentence introduction |
| SenseCAP Combo 5-in-1 Sensor with 4G | 4G environmental sensor | A ready-to-deploy, low-power device measuring temperature, humidity, atmospheric pressure, light intensity, and CO2, with 4G Cat.1 connectivity, solar-assisted power, MQTT support, and an RS485 port for expansion. |
| SenseCAP S2100 | LoRaWAN Data Logger | Connects compatible RS485 or SDI-12 instruments to a LoRaWAN network, helping existing field sensors become part of a long-range, low-power monitoring system. |
| SenseCAP 4G Data Logger | Industrial 4G data logger | Collects data from compatible wired sensors and sends it over cellular networks when a direct, wide-area connection is preferred over LoRaWAN. |
For more products, please visit the exhibition site.

See the System in Person
Whether you are evaluating a compact station, a LoRaWAN sensor network, or a 4G-connected greenhouse solution, Booth H33 is a ideal place to compare the options directly and discuss the next step for your project.
Visitors attending the in-person exhibition can also scan the QR code at the booth to apply for a sample loan. Details will be shared on site, so make sure to stop by and discover what is available for hands-on evaluation.
Event Information
- Event: Meteorological Technology World Expo 2026
- Dates: 6–8 October 2026
- Venue: RAI Amsterdam, Netherlands
- Exhibitor: Seeed Studio, professional weather sensor provider
- Booth: H33