Seeed Monthly Wrap-Up for April & May 2025: Open Innovation in Action
By Ellie Cai 10 months agoPrepare for 10 tech exploration offering expert insight, 4 weekly livestream recap, and 12 product and service showcases that will leave you in awe. Plus, check out 12 latest Seeed news and event highlights, while diving into the vibrant open-source community with 7 inspiring projects.
Hey community,
Welcome to our April & May 2025 newsletter. This month, we shed light on Open Innovation In Action, from AIoT breakthroughs and edge deployments to community prototypes and global workshops/hackathons.
Prepare for 10 tech exploration offering expert insight, 4 weekly livestream recap, and 12 product and service showcases that will leave you in awe. Plus, check out 12 latest Seeed news and event highlights, while diving into the vibrant open-source community with 7 inspiring projects. Let’s jump right in!
📚 I. In-depth Feature & Tech Exploration
01. LeRobot - Lowering the Entry Barrier to Embodied AI in Robotics
Explore how LeRobot is making EmbodiedAI more accessible than ever—through modular hardware, multimodal sensing, and plug-and-play ML pipelines:
🔹 What is Embodied AI, and why it’s the future of robotics.
🔹 Human-Based vs Model-Based vs End-to-End.
🔹 ML-Driven Control: From Imitation Learning to Sim2Real.
🔹 Developer Toolkit: Open datasets, training APIs, and Jetson-ready hardware.
02. How to use the Lekiwi in Lerobot

The Lekiwi is a fully open-source robotic car project launched by SIGRobotics-UIUC. It includes the detailed 3D printing files and operation guides, designed to be compatible with the LeRobot imitation learning framework. It supports the SO101 robotic arm to enable a complete imitation learning pipeline. Check out the wiki now.
03. Getting Start with reComputer AI Industrial R2135 Series

reComputer AI Industrial R2135 is powered by Raspberry Pi CM5 and Hailo AI accelerator, this compact edge AI system delivers 26 TOPS for real-time multi-channel vision processing. With a quad-core Cortex-A76 CPU, up to 16GB RAM, 64GB eMMC, and a versatile interface, it ensures seamless integration into industrial AI applications. More
04. Node-RED Introduction for reCamera Gimbal
This wiki provides step-by-step guidance on how to use Node-RED nodes to operate and control the motors on the reCamera gimbal. The default flow on the Device is a more comprehensive example of how you can use UI nodes with gimbal nodes, but we are going to break down the nodes one by one to explain how you can use it. Click for more.
05. Getting Started with XIAO 7.5″ ePaper Panel

Powered by XIAO ESP32-C3, this 7.5 inch ePaper display is a versatile, energy-efficient smart E Ink® screen supporting a wide range of popular community applications including Home Assistant, TRMNL, Arduino, and more. This guide will help you get started quickly and integrate the ePaper display into your own projects. Dive in now.
06. Flash SenseCAP Watcher Agent Firmware

This guide provides instructions for flashing the Watcher Agent firmware to your SenseCAP Watcher device using Espressif’s Flash Download Tool.
Special thanks to XiaoZhi AI Chatbot for their open-source contributions that made this project possible. Read more.
07. Getting Started with the Wio Tracker L1 Meshtastic Node
The Wio Tracker L1 Series is a low-power, highly extensible Meshtastic node featuring LoRa (862–930 MHz), the nRF52840 for efficient processing, and an L76K GPS module for accurate location tracking. Designed for flexibility, it supports OLED and E-Ink displays, as well as solar panels and battery power, making it ideal for a wide range of IoT and off-grid applications. Explore more.
08. XIAO RP2040 with PlatformIO

PlatformIO is a development platform that integrates many types of development boards and has good scalability. If the platform does not have the type you need, you can manually add the type of development board yourself. The code you write on Arduino can use it, just add the corresponding library. In this wiki, we wiil introduce how to install and run the sample code in PlatformIO. Click here.
09. XIAO MG24 Connect HomeAssistant With Matter

In this wiki, we will utilize the Sonoff Zigbee 3.0 USB Dongle to access the HomeAssistant and thus act as a border router, while the Seeed Studio XIAO MG24 will act as a Matter protocol device with the Thread network.for your convenience, we will take you through the following three questions to better engage in the process.Thanks to the author @tutoduino for the WiKi thoughts! Find out more.
10. Getting Started with Grove – Barometer Sensor (SPA06-003)
Grove – Temperature and Barometer Sensor(SPA06-003) is a high-precision and a low-current environmental sensor measures the temperature and barometer. It supports both I2C and SPI communication and we provide the SPA06-003 Arduino library. Learn more here.
🎬 II. Weekly Livestream: Making Next Gadget
01. What Can This Pocket-Sized Instrument Do?
We are excited to introduce the Minichord, a pocket-sized musical device that transcends traditional boundaries and provides musicians of all levels endless creative possibilities. We had a live chat with Benjamin, the mastermind behind it, to get a sneak peek into the development process and learn how Seeed Co-Create brought this product to life. Rewatch here.
02. Advanced Sensors Meets AI for Hyperlocal Weather Forecasting
How cutting-edge AI and advanced sensing technologies are reshaping weather prediction, down to the neighborhood level? In this live session, Seeed Studio and Benchmark Labs unveiled their joint hyperlocal weather forecasting solution powered by AI models and sensor-rich weather stations like SenseCAP weather stations/sensors. Rewatch here.
03. Build Your Dream Smart Home Dashboard with Seeed Displays
Still looking for a perfect display for your Home Assistant Lovelace dashboard? This livestream showcased our display solutions for Home Assistant dashboards, from the XIAO 7.5″ ePaper Panel and SenseCAP Indicator, to the powerful reTerminal and reTerminal DM. Rewatch here.
04. Building the next open-source humanoid robot!
In this livestream, we’re excited to have Shawn Shao, Founder of RobStride Dynamics, and Elaine Wu, our Head of AI Robotics, to dive into the hardware and software stack behind today’s cutting-edge humanoid robots. Rewatch here.
📰 III. Product & Service Showcases
Stay up-to-date with the latest product releases from Seeed. Discover new tools, platforms, and services designed to streamline your workflow and accelerate innovation in your projects.
01. [New] SO-ARM101 Low-Cost AI Arm Servo Motor Kit Pro for LeRobot
Meet the new SO-ARM 101 kit by Hugging Face! Built with upgraded motors and precision 3D-printed components, SO-ARM 101 is designed for developing with LeRobot, enabling full end-to-end robot learning. It’s open-source, affordable, and DIY-friendly — ideal for robot enthusiasts, developers, and researchers. Get yours today!
02. Seeed Studio IoT Button, Simplifying Your Home Automation

Seeed Studio IoT Button – an ESP32-C6-powered smart switch that brings simplicity to Home Assistant automation, features both ESPHome and Zigbee integration, customizable RGB indicators, and sustainable design with USB-C charging and replaceable battery. Read more.
03. XIAO Vision AI Camera: Compact, Smart, and Ready for Edge AI

Introducing the XIAO Vision AI Camera — a smart vision gadget built for makers, engineers, and developers looking to bring edge AI vision to life. At its core, the XIAO Vision AI Camera integrates three components — the Grove Vision AI Module V2, OV5647 5MP camera, and XIAO ESP32-C3. Click for more.
04. Bringing Hyperlocal Weather and Water Insights to German Lakeside Tourism with Seeed’s LoRaWAN Sensors
TJK-Solutions developed and deployed a fully wireless, real-time environmental monitoring system designed specifically for enhancing public safety and visitor experience in lakeside tourism areas. At the core of this solution are the Seeed Studio SenseCAP S2120 LoRaWAN Weather Station and SenseCAP S2106 pH & Temperature Sensor, seamlessly integrated to provide accurate, continuous data on both weather and water conditions in Am Mellensee, Brandenburg, Germany. Find out more here.
05. XIAO 2-Channel AC Wi-Fi Energy Meter for Smart Solar Production and Energy Monitoring

XIAO 2-Channel AC Wi-Fi Energy Meter, a powerful and flexible solution for monitoring your home’s energy production and usage. With pre-falshed ESPHome firmware running on the XIAOESP32-C6, it can monitor two independent AC circuits via Home Assistant Lovelace Dashboard. Find out more here.
06. LED Driver Board for Seeed Studio XIAO, Customizing Your Spaces with Smart LED lights

With the LED Driver Board for Seeed Studio XIAO, you can easily customize your lighting effects. Whether you’re creating ambient lighting for your room, reactive lighting for a music setup, or automated lights for smart home scenarios, this board makes it all simple and accessible. Click for more.
07. Getting start with reComputer J401B
The reComputer J401B series is an iteration on reComputer Classic series. The reComputer J4011B with NVIDIA Jetson Orin NX 8GB modules is a powerful and compact edge AI device with rich interfaces: 2x USB 3.2, HDMI, Ethernet, M.2 Key E for Wi-Fi module, M.2 Key M for SSD, mini-PCIe for LTE module, CAN, 40-pin and more. Get One Now
08. SenseCAP Solar Node: the Solar-Powered Meshtastic Device for Reliable Mesh Network Expansion

Seeed Studio introduces the SenseCAP Solar Node Series — P1 and P1-Pro — two highly integrated, solar-powered meshtastic nodes that are ideal for expanding the mesh network. These plug-and-play devices are engineered for off-grid, low-power, long-range networking, making them ideal for outdoor enthusiasts, Meshtastic developers, community responders. Read more.
09. We’ve Open-Sourced SenseCAP T1000-E for LoRaWAN and SenseCAP M2 LoRaWAN Gateway

We’ve open-sourced two key products from the SenseCAP LoRaWAN lineup: the SenseCAP T1000-E Card Tracker for LoRaWAN(not the Meshtastic version) and the SenseCAP M2 LoRaWAN Gateways. These open-source releases are especially beneficial for enterprise R&D professionals who need more than just off-the-shelf devices. Get Started Today.
10. ODM vs. OEM vs. Licensing Program: Services You Should Know from Seeed Studio’s Customization Offerings
For businesses looking to bring their unique hardware ideas to life, navigating the path from concept to production can be complex. At Seeed Studio, we partner with companies to transform their vision into tangible products. We offer a range of flexible collaboration models – Original Design Manufacturing (ODM), Original Equipment Manufacturing (OEM), and our innovative Licensing Program – each designed to meet different needs and accelerate your time to market. Learn more.
11. Orders Are Open for reCamera Gimbal!

The reCamera Gimbal 2002 Series is the first open-source camera control system with 1TOPS AI camera (reCamera) and 2-axis gimbal. Its dual brushless motors enable 360° yaw and 180° pitch for full coverage. Only $158 from June 20th to June 22nd (UTC+8), limited to one per person, hurry up and grab it!
12. Seeed XIAO MIDI Synthesizer, Making Music Instantly

As an open-source MIDI synthesizer, XIAO MIDI Synthesizer is more than just a compact device—it’s a full-fledged music creation tool in your pocket. Powered by the XIAO ESP32-C3 core and a professional-grade SAM2695 sound engine, it transforms MIDI signals into rich, vibrant soundscapes, making music creation seamless and effortless. This device is ideal for creators looking to simplify their workflow and unleash creativity. Click for more.
👩💻 IV. News & Event Highlights
Get the inside scoop on recent events and news. Gain valuable insights, key takeaways, and highlights from industry experts and thought leaders at the forefront of ML innovation.
01. Seeed Studio to Participate in FAB25 Czechia: Bridging the Gap
Seeed Studio will be joining FAB25 Czechia, the 21st annual international Fab Lab Conference & Symposium, taking place from July 4–11, 2025, in Brno and Prague. As part of this vibrant celebration of digital fabrication and maker culture, we’re bringing hands-on workshops, an interactive booth, hackathon and other exciting experience to the community! Find out more.
02. LeRobot Worldwide Hackathon
The Worldwide LeRobot Hackathon is happening June 14–15, 2025. Hosted by Hugging Face, this free global event invites developers, makers, and robotics enthusiasts to join forces—online or in local hubs—to build the future of open-source robotics as one big family. More info.
03. Join Seeed Studio Creator & Affiliate Program
Seeed is inviting content creators, project sharers, and community builders to join our Seeed Studio Creator & Affiliate Program! Explore Free product trials; Commissions on every sale you refer; Exposure through Seeed’s official channels, and more. Appy now
04. Level Up! Interactive Signage Contest 2025 – Prizes Just Got Better
Over the past months, our Interactive Signage Contest has received plenty of fun and creative projects from makers in China and around the world. To encourage more ideas to spark, we upgraded the prizes; we added another $1,700 cash prize to the pool, and inviting you to join! Join our Discord community to ask questions, get feedback, or just chat with fellow makers. Find out more.
05. Chaihuo Maker Space Global Call|“Maker Residency” Program

Chaihuo Maker Residency program is designed for global makers to live, create, and collaborate in Shenzhen — the heart of China’s hardware innovation. You will get Community Access & Tech Exchange, Full Membership Benefits, Hardware Support, Supply Chain Booster and Exposure & Resources. Join the Maker Residency Program.
06. Turn Your XIAO Projects into Reality with Fusion: 30% Off PCBA

To support creators scaling up their XIAO-based PCBA designs, our Seeed Fusion team has launched the XIAO PCBA Sponsorship Program, providing global developers with exclusive support and discounts to accelerate innovation together in the XIAO ecosystem.
If you’re working with—or planning to use—any XIAO module for your PCBA project, now’s the time to apply! Click here to fill out the form and submit your project information.
07. Maker Faire Shenzhen 2025 – Call For Makers
Last year at Maker Faire Shenzhen, we welcomed 122 amazing exhibitor teams and over 30,000 passionate visitors under the theme “Enchant Everything with AI.” So… what’s next?
This year, AI is blooming everywhere—in labs, factories, classrooms, on your wrist, and even on your smartphone! From glasses that interpret the world to robots that can feel, AI flows into our lives like water into soil—reshaping how we live, build, and dream.
And that’s exactly what we’re celebrating at Maker Faire Shenzhen 2025 — under the theme “AI and More Things.” Call for Makers is now officially OPEN!
08. Empowering Innovation with TinyMl and IoT in Buea, Cameroon

Our Ranger Dessap Loic hosted the first TinyML and IoT workshop in the vibrant city of Buea, SouthWest Region of Cameroon, at the College of Technology, University of Buea. During the workshop, 80++ students enthusiastically explored cutting-edge technologies through practical, immersive sessions. More info.
09. Ranger Program Recap: A Season of Global Impact and Growing Connections

Over the past season, our incredible Rangers have hosted over 15 events worldwide! From the hands-on IoT workshop in the Medellin community to TinyML sessions at Universidad Tecnológica de Pereira, Vimalagiri Public School, Universitas Raharja. And the meshtastic workshop at SMK Islamic Village, the energy and excitement have been amazing. More
10. Seeed Embodied AI Hackathon at GOSIM AI Paris 2025
With 30 developers joining together, collaborating with 1MS.AI and Hugging Face, we got a 2-days journey about embodied AI hackathon at GOSIM AI Paris 2025. We tackled everything from hardware assembly to dataset collection and model training, verification, and deployment, all in just under 30 hours. Stay tuned for our next embodied AI event.
11. Physical AI with reThings Jetson Orin Platform
At Seeed, we’re making robot development easier and more accessible for everyone. Explore our latest NVIDIA Jetson-powered edge AI devices and open-source robotics projects in our AI Robotics homepage. Check out now.
12. The First Home Assistant Community Day in China
The First Home Assistant Community Day in China was held in Chaihuo Makerspace on May 24! Find out more.
🌈 V. Community Project Spotlight
Celebrate the creativity and ingenuity of our community members with featured projects and ideas in machine learning. From open-source libraries to DIY solutions, there’s no shortage of inspiration to be found among our talented community.
01. Vibe AI: Wearable Nutrition Tracker Powered by Seeed Studio XIAO ESP32S3
Vibe AI, developed by Jacob Trebil, is a necklace-sized wearable that uses AI and computer vision to passively track what you eat and help you stay on track with your health goals. ith the initial version already sold out and hundreds on the waitlist, the team is now working on Vibe v2—a smaller, sleeker, and more energy-efficient evolution of the AI wellness copilot. Learn more.
02. MiniMe — A ChatGPT-Powered Digital Doppelgänger in a Tiny Box, Powered by XIAO ESP32-S3

Michael Merrifield, an emeritus professor of Astronomy in University of Nottingham has pushed the boundaries of AI-powered DIY projects with MiniMe, a pint-sized digital version of himself. Designed to be as compact as possible, this fully self-contained gadget talks like him, thinks like him, and fits neatly in a custom 3D-printed box. Learn more.
03. Zippy: The World’s Smallest Power-Autonomous Bipedal Robot, Powered by XIAO nRF52840

At just 3.6 cm tall, Zippy is redefining what’s possible in small-scale robotics. Developed by Steven Man and his research team (Soma Narita, Josef Macera, Naomi Oke, Aaron M. Johnson, and Sarah Bergbreiter) from Carnegie Mellon University, this tiny yet mighty robot is the smallest self-contained bipedal walker to date. Find out more.
04. Byte 90: A Retro-Inspired Interactive Designer Toy Powered by XIAO ESP32-S3
Developed by Alex Vong of ALXV Labs, Byte 90 is a 3D-printed, retro-inspired interactive designer toy that captivates both the eyes and the imagination. Built on the Seeed Studio XIAO ESP32S3, this collectible not only pays homage to iconic tech designs of the past but also lays the foundation for creative expansion. Learn more.
05. Porting the ReSpeaker 2-Mics Pi HAT v2 to BeagleY-AI
We’re thrilled to spotlight a project that brings together Seeed Studio’s ReSpeaker 2-Mic Pi HAT v2 and the powerful BeagleBoard.org Foundation’s BeagleY® AI SBC — opening up exciting possibilities for voice interfaces and intelligent applications at the edge. Learn more.
06. Cardiogram – a Portable ECG Device for Daily Use on the Go
Cardiogram—a portable ECG wearable powered by the XIAO ESP32C3, streams real-time heart data via BLE to a SwiftUI mobile app, making heart health monitoring as accessible as tracking steps or body temperature. Find out more.
07. ANAVI Miracle Emitter: An Open Source RISC-V Board to Light Up Your World Powered by XIAO ESP32-C3
ANAVI Miracle Emitter is a compact, open-source development board designed for LED control, home automation, and smart lighting created by ANAVI Technology. Powered by Seeed Studio XIAO ESP32-C3 microcontroller running RISC-V architecture, it offers built-in Wi-Fi and Bluetooth 5 (LE) capabilities. Check it out.
That’s all for today, thank you all for reading through this April & May 2025 Monthly Wrap-up in your spare time. If you wanna share what projects you’re working on, shoot us a tweet @seeedstudio, let us know on LinkedIn and Discord, or publish your project on our Project Hub on Hackster.
#Notes
If you’re new to this session, here is a brief intro. We have gotten dozens of requests over the years for a Seeed Monthly Newsletter. Although we already have a newsletter for weekly updates, we still need a place to host overall information about what’s happened on a monthly basis. It can offer an efficient and friendly way to get updated for the whole community. And that’s what we expect for our Seeed Monthly Wrap-ups. Instead of putting it as a subscribe-to-read format, we’re publishing them on our blog, so as to keep it as open and accessible as possible for the whole community. For each entry, we will cover awesome projects from the community, campaigns that we are running, new products, IIoT Solutions, and even secret recipes for prototyping and manufacturing.
Previous Monthly Wrap-ups: